Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Product List
AD5933-Slide35

Also, the system clock is used by the internal ADC to digitize the response signal and requires 16 clock periods to perform a single conversion. Therefore, with a maximum system clock frequency of 16.776MHz, the ADC can sample the response signal with a frequency of 1.0485MHz (i.e. a throughput rate of ≈1.04 MSPS). The ADC will convert 1024 samples and pass the digital results to the AD5933 MAC core where it performs a 1024 point DFT to determine the peak of the response signal at the ADC input.

PTM Veröffentlicht am: