Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Product List
AD5933-Slide30

However, it is also important to note that the corresponding DC bias voltage will also scale with the choice of output excitation voltage. Also, the receive side is always hard biased at VDD/2. The problem is that the shift in DC bias may cause the internal I-V on the receive side to saturate based on the RFB/Z value in question. If the ratio is sizeable, results outside the rails of the I-V amplifier are possible.

PTM Veröffentlicht am: