Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Product List
AD5933-Slide14

The Start Frequency is a 24-bit word that is programmed to the on-board RAM at addresses 82h, 83h, and 84h. The required code loaded to the START FREQUENCY register is based on the master clock frequency and the required Start Frequency output from the DDS as follows: Start Frequency code = ( Required output start frequency/ (MCLK/4) ) x 227.

PTM Veröffentlicht am: