Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Product List
AD5933-Slide17

The Number of Increments is a 9-bit word that represents the number of frequency points in the sweep. The number is programmed to the on-board RAM at addresses 88 h and 89 h. The maximum number of points that can be programmed is 511. For example, if the sweep needs 150 points, the user programs 00 hex to Register 88 h and 96 hex to Register 89 h. Once the three parameter values have been programmed, the sweep is initiated by issuing a Start Frequency Sweep command to the CONTROL register at addresses 80 h and 81 h.

PTM Veröffentlicht am: