Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Product List
AD5933-Slide27

The above external amplifier will attenuate the peak-to-peak excitation voltage at Vout by suitable choice of resistors R1 and R2, thereby reducing the signal current flowing through the impedance. This will also minimize the effect of the output series resistance in the impedance calculations. The impedance in the above circuit under test (Zunknown) will now see the output series resistance of the external amplifier, typically much less than 1Ω, with feedback applied depending upon the op-amp device used (e.g. AD820,AD8641,AD8531) the load current, bandwidth and Gain.

PTM Veröffentlicht am: