Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Product List
AD5933-Slide12

The receive stage comprises a current–to-voltage amplifier, followed by a programmable gain amplifier (PGA), an anti-aliasing filter, and an ADC. The unknown impedance is connected between the VOUT and VIN pins. The first stage current-to-voltage amplifier sets the VIN pin as a virtual ground with a DC value of VDD/2. The signal current developed across the unknown impedance flows into the VIN pin and develops a voltage signal at the output of the current-to-voltage converter.

PTM Veröffentlicht am: