Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Product List
AD5933-Slide13

The gain of the current-to-voltage amplifier is determined by a user-selectable feedback resistor connected between Pins 4 (RFB) and 5 (VIN). It is important for the user to choose a feedback resistance value which, in conjunction with the selected gain of the PGA stage, maintains the signal within the linear range of the ADC (0 V to VDD). The PGA allows the user to adjust the output gain of the current-to-voltage amplifier by a factor of 5 or 1 depending upon the status of Bit D8 in the CONTROL register. The signal is then sent through a low-pass filter and presented to the input of the 12-bit, 1 MSPS ADC.

PTM Veröffentlicht am: