Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Product List
AD5933-Slide28

The key point is that the output impedance of the external amplifier in the above circuit, which is also in series with the impedance under test (Zunknown), has a far less significant effect on the AD5933 calibration and subsequent impedance readings in comparison to connecting the small impedance directly to the Vout pin (and directly in series with Rout). The external amplifier buffers the unknown impedance from the effects of the output series resistance of the AD5933 (Rout) and introduces a smaller output impedance in series with Zunknown.

PTM Veröffentlicht am: