Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Product List
AD5933-Slide29

In the above example application, the user wants to measure an impedance over the range of 90Ω to 110Ω using Range 4 which, in this case, generates a sine wave of 0.198V peak-to-peak amplitude independent of the impedance range measured. It may not be possible to measure the output series resistance (Rout) directly, therefore, an extra amplifier circuit, like that shown above, may be added in the signal path of the AD5933. However, the chosen external amplifier must have a sufficiently low output series resistance over the bandwidth of interest in comparison to the impedance range under test.

PTM Veröffentlicht am: