Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Product List
AD5933-Slide25

The impedance limits must be known in order to correctly calibrate the system. In the above example, the Gain Factor calculated at the mid-point frequency of 31KHz can be used to calculate any impedance in the 180KΩ to 220Ω region. Impedance results will degrade if the unknown impedance span is large or if the frequency sweep is large. If any of the calibration system gain settings change, the user will need to recalibrate the AD5933 and recalculate the Gain Factor. (See the AD5933 datasheet for further details).

PTM Veröffentlicht am: