Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Product List
AD5933-Slide18

It is important to note that the real and imaginary components stored are the real and imaginary Discrete Fourier Transform (DFT) component and NOT the real and imaginary impedance components. The DFT that is used to measure (detect) the peak signal through the system also has a real and imaginary component. The real and imaginary components of the impedance are calculated from the absolute impedance |Z| and the impedance phase angle: i.e., Rz = |Z|COS(θ) and Iz = |Z|Sin(θ).

PTM Veröffentlicht am: