Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Product List
AD5933-Slide24

When calculating the GAIN FACTOR, it is essential that the receive stage is operating in its linear region. This requires careful selection of the excitation signal range, current-to-voltage gain resistor and PGA gain. The peak-to-peak voltage presented to the ADC input is 2 V p-p. However, had a PGA gain of ×5 been chosen, the voltage would saturate the ADC. The GAIN FACTOR must be recalculated for a change in any of the following parameters: current-to-voltage gain setting resistor, output excitation voltage, or PGA gain.

PTM Veröffentlicht am: