Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Product List
AD5933-Slide15

For example, if the user requires the sweep to begin at 30 kHz and has a 16MHz clock signal connected to MCLK, the required programming code programmed is: Start Frequency code = (30KHz / (16MHz/4) ) x 227 = Hex 0F5C28. The user then programs 0F hex to Register 82 h, 5C hex to Register 83 h, and 28 hex to Register 84 h.

PTM Veröffentlicht am: