Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Product List
Cyclone-Slide9

In this video format converter example, the system must accept four independent video streams, perform video processing and format conversion and then output the new, transformed, video to at least two different downstream systems at different interfaces and have a PCI express link. This entire video processing system can be implemented in a single quad – using only four transceiver channels since the transmit and receive per channel can support independent data rates. This means that in a Cyclone® IV GX device an entire quad is available for the PCI express link required, and potentially has room for more, such as a gigabit Ethernet link.

PTM Veröffentlicht am: