Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Product List
Cyclone-Slide43

Cyclone® IV devices have eight separate banks, each of which can interface to any I/O standard or external memory. Certain banks are optimized for highest performance for memory interfaces and LVDS communication. For example, top and bottom banks are optimized for memory interface performance and left and right banks are optimized for LVDS performance. Two additional registers in the I/O cell increase DDR interface performance by improving the write margin. Differential output buffers not only reduce board space required, but also eases PCB routing in applications such as the many high volume display column drivers. The Cyclone® IV GX transceivers have dedicated I/O pins and banks which are shielded from general purpose I/O for the best performance and signal integrity. Cyclone® IV devices allow selection of 25 Ω or 50 Ω series termination values. The user can also choose to have these values calibrated at power up before going into user mode. A periodic user mode calibration feature may be offered after device characterization. Adjustable slew rates can improve signal integrity by slowing down edge rates on non-performance critical I/O pins.

PTM Veröffentlicht am: