Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Product List
Cyclone-Slide17

Shown on this slide is the block diagram. The transceivers which also can be used for non-PCI express applications are shown on the right. The interface to the hard IP block supports a PIPE 2.0 compliant interface. This hard IP PCI express block offers support for endport and rootport applications and, as can be seen, implements a complete protocol stack. If the customer needs the flexibility, different layers can be bypassed as shown in the block diagram, e.g. for an application which needs a custom solution for the transaction layer. The PCI express hard IP is similar to that in the Arria® II GX and Stratix® IV GX which have successfully passed PCI SIG compliance testing.

PTM Veröffentlicht am: