Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Product List
Cyclone-Slide7

The next few slides will present specific examples of how the Cyclone® IV GX transceiver architecture can allow the user to implement multiple protocols efficiently. PCI express and Ethernet, specifically gigabit Ethernet, are ubiquitous these days. A simple design requiring a PCI express interface and an Ethernet connection can be implemented in as little as two channels. In a larger system, a multi-lane PCI express channel with channel bonding and multiple gigabit Ethernet channels could be implemented in a single quad due to the clocking flexibility.

PTM Veröffentlicht am: