Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Product List
Cyclone-Slide10

This slide shows that MPLLs may also be shared with the FPGA core. Shown is the left half of the clocking architecture of larger devices that have eight transceivers. The top and bottom MPLLs provide three additional clocks to the global clock multiplexer and the middle MPLLs provide two additional clocks for up to twelve different clock frequencies that can be fed from these sets of PLLs. One item to note is that not all MPLLs and GPLLs can be shared. Only the adjacent MPLL can be borrowed by a quad and only one GPLL can be borrowed by a quad, but not both. It is also important to note that when the MPLLs are used to drive transceivers the clock outputs provided to the GCLK multiplexers have frequencies related to the M and N values required for the transceiver protocol.

PTM Veröffentlicht am: