Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Product List
Cyclone-Slide5

The diagram on this slide shows the sub-blocks within both the PMA and PCS. Depending on the protocol implemented, the appropriate sub-blocks will be selected when the transceiver is instantiated through the Intel® MegaWizard®. In the case of a proprietary protocol, indicated as “basic mode” in the Intel® terminology, the data path can be customized in the PCS by specifically bypassing certain functions such as the byte serializer, deserializer, the 8b/10b encoder/decoder, the rate matcher and word aligner. The only required blocks in the PCS are the functions used for de-skewing data and buffering required to successfully interface to the FPGA fabric.

PTM Veröffentlicht am: