Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Product List
Cyclone-Slide33

The PLLs in the Cyclone® IV FPGAs have four different operational modes. Source synchronous mode provides a clock-to-data relationship at the input pin (setup/hold), maintained at the IOE register. The no compensation mode is used to maintain the best jitter performance. Normal mode fully compensates the input clock delay for alignment with the clock at the IOE or core register. Lastly, the zero delay buffer mode ensures that the input clock is aligned with the dedicated external clock output.

PTM Veröffentlicht am: