Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Product List
Cyclone-Slide8

In the case of interfacing with ADCs and DACs, the specific advantage of the Intel® architecture is that it is possible to transmit and receive at different, independent, rates within each channel. With the Cyclone® IV GX, this could be implemented in as little as four channels. In fact, even more data rates can be implemented in this quad if a PLL were borrowed, as shown in the next example.

PTM Veröffentlicht am: