Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Product List
QuickSense C8051F990 Low Power MCU with Capacitive Sensing Slide 8
Continuing the discussion of the operating modes of the MCU, the next mode is the suspend mode. In suspend mode the CPU does not execute instructions and all internal oscillators are disabled to further reduce power. Some peripherals that can operate autonomously can be used, such as the capacitive sensing module and the ADC. Once again the names vary between vendors and the data sheet should be carefully examined to find the equivalent modes. Finally, the sleep mode is the lowest power mode as it turns off all system and peripheral clocks as well as power to many of the peripherals. This mode can use the integrated RTC to periodically wake the device or an external event can be used to wake the MCU.
PTM Veröffentlicht am: