Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Product List
QuickSense C8051F990 Low Power MCU with Capacitive Sensing Slide 40
The dimmer demo mode allows the user to set the LED brightness. If the MAX LED is lit, the dim level is set at maximum brightness. If the MIN LED is lit, the dim level is set at minimum brightness. The LED brightness set by the dimmer demo is preserved and used throughout all three modes. To enter dimmer mode from the slider demo mode, pinch the slider twice and wait for the “Mode 2: Dimmer Demo” LEDs to stop blinking. Then, touch the slider at the desired position to set the LED brightness. The selected position will be saved five seconds after removing the finger from the slider. At that time, the system will automatically switch back to the slider demo mode.
PTM Veröffentlicht am: