Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Product List
QuickSense C8051F990 Low Power MCU with Capacitive Sensing Slide 37
In the slider demo, the LED will track finger position on the slider for a slowly moving finger. If the finger performs a gliding motion across the slider, then the LED will continue moving in the direction of the glide. The LED will act as a ball in motion and will continue rotating until it is stopped. The LED may be stopped by pressing one finger on the slider. If two fingers are placed on the slider, the LED will stop faster. If the finger generates additional fast gliding motions on the slider, then the enabled LED will start rotating faster through the bank of LEDs. If left alone, the rotating LED will slow down until it comes to a complete stop. This simulates the force of friction on a moving ball.
PTM Veröffentlicht am: