Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Product List
QuickSense C8051F990 Low Power MCU with Capacitive Sensing Slide 12
When comparing device specifications it is important to consider the conditions used to derive the parameters provided. Silicon Labs provides all of its device specifications over the full operating voltage and temperature. There is no derating required when looking at the specifications. In many cases, suppliers will only provide the specification at room temperature which makes it look satisfactory on paper, but further investigation reveals that it may actually be less than satisfactory.
PTM Veröffentlicht am: