Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Product List
QuickSense C8051F990 Low Power MCU with Capacitive Sensing Slide 29
In the previous example it was shown that a single element of a slider can be used as a single touch. Shown in this slide is a more complex gesture implemented using multiple elements to make up the slider. Sliders are useful for inputs such as a volume control or any input that requires a plus/minus adjustment (i.e left/right balance). The slider uses a single finger that traverses the pads as shown in the figure. The architecture of the pads is set such that when the finger crosses a boundary between two pads there is a change in both of the selected channels. This can be seen by the plot highlighting the change in counts as the finger crosses each of the boundaries. The firmware can make position determinations based on the capacitance values of the adjacent pads across the slider.
PTM Veröffentlicht am: