Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Product List
QuickSense C8051F990 Low Power MCU with Capacitive Sensing Slide 14
In the past it was assumed that a fast wake-up time meant low power. However, in reality it is the activity profile that will govern the overall system power usage. In most low power systems the device needs to perform some operation and go into a sleep mode. It is during this sleep mode that the current consumption is at a minimum. Therefore, it is desirable to remain in the sleep mode for the majority of the time, thus the overall average current consumption will be reduced. There are two ways to achieve the goal of remaining in the low power state most of the time.  Fast wake-up time is one method, fast execution time and autonomous peripherals is another. To minimize the area under the average current curve, decreasing active time is better than decreasing peak current because no matter how much the peak current is decreased, it will not be as efficient as switching to an inactive mode. Some reasons include bias currents, leakage current, etc.
PTM Veröffentlicht am: