Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Product List
QuickSense C8051F990 Low Power MCU with Capacitive Sensing Slide 18
The successive approximation, or SAR, method of measuring self-capacitance uses a pair of current sources to drive current into separate capacitors. The first is the reference capacitor, denoted as CREF; the second is CSENSOR, the sensor capacitor. The reference current source, which is denoted as IREF, is a fixed current used to drive the CREF capacitor, to provide a constant ramp voltage. The second current source, denoted ISENSOR, sources a variable current to the sensor capacitor.  After each measurement cycle the SAR logic will change the value of ISENSOR, attempting to make the ramp rate the same as the reference capacitor.
PTM Veröffentlicht am: