Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Product List
QuickSense C8051F990 Low Power MCU with Capacitive Sensing Slide 11
Frequency sensitivity is a specification that often times is overlooked. This specification provides an indication of how efficient the MCU will be when it is active and drawing the most current.  Not all MCU manufacturers follow the same curve for frequency sensitivity so it is important to check the data sheets in order to make valid comparisons. For example, the frequency sensitivity of the C8051F99x is less than 150 μA/MHz at 24.5 MHz. Comparison reveals that some competing devices cannot operate at that frequency; if they can, the frequency sensitivity goes up which consumes more current. Competing devices may claim low frequency sensitivity numbers, however, that efficiency comes from a much lower frequency. The lower frequency increases the ON time which requires all of the other system components to be active as well. This is one of the aspects of low power design that is not always obvious when choosing an MCU, but is a very important consideration.
PTM Veröffentlicht am: