Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Product List
QuickSense C8051F990 Low Power MCU with Capacitive Sensing Slide 19
As with the relaxation oscillator, when using capacitive sensing, the PCB trace acts as one plate of the capacitor. When a finger comes into proximity with the plate, it acts as the other plate and air is the dielectric. As the finger moves closer to the pad the capacitance changes based on the equation for capacitance as shown in an earlier slide. Keeping in mind that as the finger moves closer, the value for “d” is reduced which then increases the capacitance. Likewise, as seen in the previous slide, with the SAR operation as capacitance increases the comparison point for the threshold voltage decreases.
PTM Veröffentlicht am: