Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Product List
powerSPIN Motor Control ICs Slide 4

ST is making a strong focus on dual H-bridge products and stepper motor. After the release the L6470, also known as dSPIN, in HTSSOP, ST introduced a version of the same part in Power SO package for people that need better heat dissipation. If even higher voltage is required, the L6480 is very similar to the L6470 but without transistors integrated, using external MOSFETs. ST has the L6474, which is a low end version of the L6472, a current controlled version of the L6470, with less programming features. ST also has as new products, the powerSpin Half Bridge Gate Drivers in QFN package and the smartDRIVE family (L639x).

PTM Veröffentlicht am: