Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Product List
powerSPIN Motor Control ICs Slide 3

A motor control system is composed of three main elements: the controller, that handles motion management, and includes the logic and analog circuits that generate switching patterns to drive the power switches, the gate driver, that drives the power switch array, and the power stage array, where solid stage switches transfer the power to the motor, these could be IGBTs or MOSFETs. A monolithic motor driver is a device integrating the full power stage and in some cases, also the controller in a single chip. The main advantage of the high level of integration is reduced part count, with the inclusion of protection and diagnostics resulting in devices that are robust, highly reliable and easy to use. So a monolithic solution offers a lower system cost, a smaller PCB and higher reliability and performance.

PTM Veröffentlicht am: