Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Product List
powerSPIN Motor Control ICs Slide 22

Shown here is the PWM modulator technique, with two different current decay modes that are possible, the slow decay and fast decay. It is possible to change the decay mode by means of the logic level applied on a dedicated pin. In fast decay mode, the voltage applied to the winding of the motor is reversed during off time. The discharge time is fast because the voltage applied to the motor winding is close to the full voltage supply, but with reversed polarity with respect to the on time. In slow decay mode, the motor winding is instead short-circuited to the voltage supply, and the discharge time of the motor winding is slow because the voltage across it is almost zero.

PTM Veröffentlicht am: