Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Product List
Fundamental-Slide9

As stated previously active probes are based on transistors. Due to the very high input resistance and very low capacitance active probes are very useful for high frequency applications. The output impedance of the active probe must be matched to the oscilloscope, at 50 Ω. When the active probe is connected to the oscilloscope it automatically selects the coupling to 50 Ω. In the 50MHz to 1GHz range it is important to keep capacitance low, typically the active probe is a very low 0.5pF to 1.5pF.

PTM Veröffentlicht am: