Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Product List
Fundamental-Slide35

Common mode rejection ratio changes with frequency. As shown in the graph on this slide, the top trace is the high performance differential amplifier; the red trace is the passive differential probe. As can be seen, as the frequency goes up, the CMRR goes down in both scenarios. The performance is better with the amplifier, the DA1855, it is better at the low frequency end and remains better overall.

PTM Veröffentlicht am: