Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Product List
Fundamental-Slide39

The Hall effect device is the most popular current measuring method. It has a magnetic core and a shunt is needed to clamp the current probe across. It does measure AC and DC; it is pretty easy to attach to the circuit, and the cost is moderate. The Hall effect probe is powered by the oscilloscope; this slide shows the little amplifier that is inside the probe. In some cases it may be necessary to add a shunt, an access wire, and it does insert some impedance into the circuit under test. A wider bandwidth current probe can be produced by combining a conventional current transformer with a Hall Effect device to measure DC. A passive filter circuit is added to the Hall effect amplifier to carefully control the upper bandwidth to align with the lower bandwidth of the current transformer, providing relatively flat frequency response from DC to moderate frequencies. As with the DC current probe, a silicon Hall effect device is generally used to reduce gain error over temperature. While they are moderate cost, these probes tend to have low sensitivity.

PTM Veröffentlicht am: