Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Product List
Fundamental-Slide33

This slide shows a high performance differential amplifier with both inputs connected to the source. On the previous slide the scope is set to 1V per division, showing about 5V common mode signal. Using a high gain differential amplifier on the same signal the common mode voltage is greatly reduced. On this slide the scope is still set to 1V per division and the common mode is down to approximately 1V.

PTM Veröffentlicht am: