Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Product List
Fundamental-Slide5

Oscilloscope coupling is an important consideration. The oscilloscope can have an internal 50Ω termination which could cause excessive attenuation if applied improperly. Most modern probes have a sense pin that mates with a sense ring on the scope. This will automatically set the correct coupling and attenuation factor.

PTM Veröffentlicht am: