Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Product List
Fundamental-Slide24

One alternative to floating the scope is called quasi-differential or channel A minus channel B. The signal is acquired by using two vertical channels and subtracting the difference either in the analog domain, or using waveform math in a digital scope. Notice that the scope ground lead is not used in the measurement. This technique overcomes some of the problems with floating the scope. The scope remains safely grounded and the load is not exposed an unbalanced capacitance on either input. However, channel A minus channel B does not work effectively in situations where the signal being measured is smaller than the common mode signal being rejected, such as an upper gate drive measurement or the voltage measured across the current shunt as shown in the example on this slide. In these applications, the user is asking the scope to measure a small difference between two large signals. Small errors in gain accuracy of the one channel relative to the other can be larger than the difference the user is trying to measure.

PTM Veröffentlicht am: