Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
Intelligent Power Switches Slide 30

The SPI bus of the VNI8200 allows the daisy chain configuration, in other words, several VNI8200 can be put on the same bus. The daisy chain allows to save a lot of pins on the microcontroller. With 36 actuators in parallel mode, 36 pins of the microcontroller are necessary. In fact, even more if diagnostics are used. Thanks to the daisy chain configuration of the SPI bus, only 4 pins are necessary.

PTM Veröffentlicht am: