Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
Intelligent Power Switches Slide 20

In red are the products released in 2012, the VNI2140 and the VNI4140. The VNI8200XP was released in Q2/2013, the ISO8200B should be released Q3/2013. The L6362A is replacing the L6362 that will not be put in production. The L6362A is a low cost and simplified version of the L6362. All the new products are with multi-channel IPS. The VNI2140. that was released in 2012 is a two channels while the VNI4140 is a 4 channel IPS. The VNI8200 has 8 channel like the ISO8200 that integrates the isolation too. The L6362A is the slave side for the I/O link protocol.

PTM Veröffentlicht am: