Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
Intelligent Power Switches Slide 27

As shown on this slide, for all the VIPower family, the outputs can be put in parallel. That means a large number of combinations are available. In the previous slide, the VN751 was shown as having the smallest RDSON with 60 mOhm. This is true if only one output is used. If a customer need a 20 mOhm IPS, there is in fact a solution. All the multi channel IPS can have their outputs in parallel. So, the product like the VNI4140 that has 4 channels and an RDSON 0f 80 mOhm per channel can be configured as a single channel IPS with 20 mOhm. The decrease of the RDSON allows at the same time to increase the current driving a load.

PTM Veröffentlicht am: