Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
Intelligent Power Switches Slide 11

For instance, with a 15k Ohm resistor, the current limit is 1 A and with a 5k Ohm resistor, the current limit is 3 A. This is the highest value that can be programmed. With a resistance below 5k Ohm, the max output current will be 3.2 A, so there is a short circuit protection, even if the value of the resistor is too low or wrong for any reason.

PTM Veröffentlicht am: