Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List Associated Content
Types of Power Devices Based on Application and Voltage/Current Range Image of ROHM's Power Devices by Application and Voltage/Current Range

ROHM manufactures many types of power devices that can be used for the various industrial motor applications mentioned in the previous slides. Products should be selected depending on the input voltage range, motor current range, type of application, and package requirements. The next slides will explain the power devices listed on this page in greater detail.

PTM Veröffentlicht am: