Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Product List
Small Motor Drivers Slide 9

Looking at the block diagram for the L6506 you see two fixed frequency PWM circuits plus the logic to combine the PWM signal with the phase information from the step generator and then feed that to the two power bridges. The peak motor current is regulated by sensing the voltage across the resistor on the Vsense inputs and comparing it to the reference input. When the voltage at the Vsense input reaches the reference voltage, the comparator will reset flip-flop that will cause the PWM to turn the bridge off. The oscillator sets the flip-flop at a fixed frequency and the cycle repeats. Generally the L6506 is connected to the phase inputs of the power bridge so it typically implements phase chopping or slow decay mode chopping in the bridge.

PTM Veröffentlicht am: