Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Product List
Small Motor Drivers Slide 11

The main difference between this device and the L6506 is that it takes a clock input from the microcontroller rather than the four phase inputs. The translator block is a state machine that generates the phases for full step or half step drive for a stepper. The current control works in the same way as the L6506. The phase and enable outputs from the translator are combined with the PWM by the logic block. The control input selects either fast decay, feeding the PWM on to the enable pins, or slow decay, feeding the PWM onto the phase pins.

PTM Veröffentlicht am: