Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Product List
Small Motor Drivers Slide 32

The L6221 has four phase inputs plus an enable input with logic to drive the four Darlington output transistors. Notice that the inputs are true logic inputs and not directly the base or base resistor like the ULN2000 series. The device also integrates the diodes for the clamp circuit and needs only the external Zener.

PTM Veröffentlicht am: