Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Product List
Small Motor Drivers Slide 29

Choosing the correct value for the Zener in the clamp circuit is important. Remember that both halves of the coil are wound on the same piece of iron so there is some transformer coupling between the two halves. When the left transistor is on, the right transistor will have a voltage equal to twice the supply voltage on its collector due to this transformer action. So the clamping voltage must be something greater than twice the power supply voltage or energy will be transferred from the power supply to the clamp.

PTM Veröffentlicht am: