Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Product List
IGBT and SLLIMM IPM Slide 35

Features of the low cost FM, Full Molded package, devices are presented on this slide. These devices are made of a DIP epoxy molded construction. These devices all use Trench Gate Field Stop IGBT technology and have improved soft recovery freewheeling diodes. As mentioned previously, the NTC temperature sensing option is now located on the power side, near the IGBTs. They also include the smart shutdown feature that was introduced in some of the earlier Gen 1 SLLIMM products.

PTM Veröffentlicht am: