Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Product List
IGBT and SLLIMM IPM Slide 32

Shown on this slide are the four package options for SLLIMM Gen2 devices based on two variations of lead frame and two variations of thermal interface. FM stands for Full Molded epoxy packaging and DBC stands for Direct Bonded Copper substrate. The FM package is good for low cost solutions but not as effective at conducting heat away from the IGBTs inside as the higher cost DBC package is.

PTM Veröffentlicht am: